※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
Design & Development
Innovation Centre
At the Toshiba Innovation Centre we constantly strive to inspire you with our technologies and solutions. Discover how to place us at the heart of your innovations.
Knowledge
Highlighted Topics
Further Materials
Other
This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Do not apply a voltage exceeding the rated emitter-base voltage (VEBO) shown in the Absolute Maximum Ratings table (Table. 1) to the base terminal (negative bias in the case of npn transistors and positive bias in the case of pnp transistors). Doing so will degrade hFE and other parameters.
Bipolar transistors have the highest concentration in the emitter, followed by the base, then the collector. The concentration of the emitter is over 100 times higher than that of the base. The higher the concentration, the lower the withstand voltage tends to be.
VEBO has only a few volts. Care must be taken when inputting a large-amplitude signal to the base. In addition, reverse bias is applied to some circuits such as the circuit below. Please consider the usage conditions when designing.
When a monostable multivibrator is composed of bipolar junction transistors (BJTs), a bias voltage exceeding the rated VEBO might be applied to the base.
The following describes the operation of the multivibrator shown in Fig. 1.
The following documents also contain related information: