※  : Products list (parametric search)
※  : Products list (parametric search)
※  : Products list (parametric search)
※  : Products list (parametric search)
※  : Products list (parametric search)
※  : Products list (parametric search)
※  : Products list (parametric search)
※  : Products list (parametric search)
This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
If the seat of the general-purpose logic IC does not contain a description of the maximum operating frequency, the propagation delay time (tpLH, tpHL) can be roughly estimated using the following formula. Maximum operating frequency ≒ 1/ (tpLH + tpHL)
Table 1 shows the propagation delay times of representative products in each series and the results of the above formula.
Propagation delay times depend on the IC function. For ICs other than the typical ICs shown below, see the datasheet for propagation delay times and use them to calculate the maximum operating frequency. Propagation delay times also depend on wire lengths and loads in actual applications.
 The maximum operating frequencies shown below should be considered only as a guide. Be sure to verify that the ICs you have selected operate properly under actual usage conditions.
| Type | Series Name | CMOS Logic IC Series No. | One-Gate Logic ( L-MOS ) Equivalents | Operating Voltage Range | Output current*2, IOUT (mA) | tpLH ,tpHL( ns )*1 CL = 50pF | Maximum Operating Frequency (Calculated value) (MHz) | 
|---|---|---|---|---|---|---|---|
| For 5-V Systems | Standard | 3 to 18 | ±0.51 | 200 | 3 | ||
| High Speed | 2 to 6 | ±4.0 or ±6.0 | 23 | 22 | |||
| 4.5 to 5.5 | 31 | 17 | |||||
| Advanced | - | 2 to 5.5 | ± 24 | 8.5 | 59 | ||
| 4.5 to 5.5 | 9.0 | 56 | |||||
| Very High Speed | 2 to 5.5 | ± 8.0 | 8.5 | 59 | |||
| 10 | 50 | ||||||
| 9.5 | 53 | ||||||
| 4.5 to 5.5 | 8.5 | 59 | |||||
| For low voltage Systems | Low Voltage | 1.8 to 5.5 | ± 16 | 6.5 | 77 | ||
| Very Low Voltage | 1.65 to 3.6 | ± 24 | 4.2 | 114 | 
*1: Maximum propagation delay time of typical ICs (TC4001, TC74HC244, TC74HCT244, TC74AC244, TC74ACT244, 74VHC244, 74VHC9541 (An-Yn), VHCT244, VHCV244, 74LCX244, and TC74VCX244) at -40 to 85 °C, except for the TC4001 for which the maximum propagation delay time at 25 °C is shown.
*2: Those output current values are from DC Characteristics table of the datasheet. In addition, absolute maximum ratings also specify the current.
The following documents also contain related information.