PFC Circuit Design with the Online Simulator

Interleaved PFC Circuit Configuration and Key Design Considerations

Please Login to view more detailed articles.
Click here to Login

Introduction - Why PFC Circuits Need to Be Considered in the Early Design Stage

In an AC-DC power supply, distortion of the input current causes heating of wiring and components and injects harmonic currents into the power line.
Such impacts on the power line are difficult to mitigate at a later stage, even if the downstream (DC-DC) stage is optimized. Therefore, the design approach must be determined at the primary (input) stage.
In addition, harmonic current is limited by international standards*1, which define the allowable harmonic current that equipment can inject into the power line.
To address this issue, a power factor correction (PFC) circuit is used. A PFC circuit is an essential element that should be considered at the early stage of design, not only to improve efficiency but also to ensure compliance with standards.

*1: IEC 61000-3-2 (≤16A per phase), IEC 61000-3-12 (>16A to ≤75A per phase), etc.

What Does a PFC Circuit Improve?

In a conventional rectifier and smoothing circuit (bridge rectifier with a smoothing capacitor), the input current flows in pulses near the peaks of the AC voltage, and the current waveform deviates from a sinusoidal waveform.
As a result, even for the same output power, the RMS value of the input current increases, causing heating of wiring and components and injecting harmonic currents into the power line.
A PFC circuit controls the input current in synchronization with the input voltage, bringing the current waveform closer to a sinusoidal waveform and reducing the phase difference between voltage and current. This improves the power factor and reduces harmonic current.

Basic Concept of Switching PFC

In modern PFC circuits, a switching method using MOSFETs is commonly used. An inductor and switching devices are used to control the current in accordance with variations in the input voltage.
In switching PFC, key design considerations include the switching condition of the inductor current and how the current ripple and peak current vary.

PFC Circuit Topologies

PFC techniques vary by circuit configuration and are selected according to application, power level, and efficiency requirements. In the Online Simulator, the following topologies are available as the input stage (PFC stage) of an AC-DC power supply.

  • Single PFC: Single-phase boost PFC (basic topology)
  • Interleaved PFC: Two-phase PFC (current sharing and reduced ripple)
  •  Totem-Pole PFC: A topology in which MOSFETs perform both rectification and PFC operation
  • Semi-Bridgeless PFC: A bridgeless configuration that retains some diodes
Category Topology  Key features Typical applications/positioning
Passive Passive PFC Uses a reactor to suppress input current variation; simple but relatively large Low-power and simple power supplies
Active Single PFC Single-phase boost PFC; basic topology with the simplest circuit configuration  Basis for small- to medium-power supplies
Interleaved PFC Two-phase current sharing, reduced ripple, and improved thermal distribution  Medium- to high-power supplies
Totem-pole PFC Uses MOSFETs for both rectification and PFC operation to improve efficiency  High-efficiency power supplies
Semi-bridgeless PFC Partially reduces bridge loss while retaining some diodes  Applications aiming at higher efficiency with moderate complexity
Bridgeless PFC Eliminates the input bridge to reduce conduction losses  High-efficiency and high-power applications

Switching Conduction Modes (CCM/CRM/DCM)

In PFC circuits, there are multiple options for how current is conducted. Active PFC circuits are divided into three types according to the current conduction mode used: continuous conduction mode (CCM), critical conduction mode (CRM), and discontinuous conduction mode (DCM).
In CCM, current flows continuously, enabling input current shaping.
Since waveform characteristics such as ripple, peak current, and distortion directly affect design decisions, it is important to check the waveform not only from the topology point of view but also from the conduction mode point of view.

Mode Features Impact on design
CCM (Continuous Conduction Mode) Current does not become discontinuous/small ripple Suitable for large-capacity power supplies/switching loss design is important
CRM (Critical Conduction Mode) Switching occurs when the inductor current drops to zero Good balance between loss and efficiency
DCM (Discontinuous Conduction Mode) Current becomes zero every cycle Suitable for low-capacity power supplies/high peak current

What Can Be Verified Using the Online Simulator?

The Online Simulator allows users to verify input current waveforms, differences in current ripple and peak current among circuit topologies, and operating waveforms when MOSFETs or circuit parameters are changed.
In addition, the simulator displays waveforms after setting the conditions and enables comparison of waveforms, making it effective for preliminary verification in the early design stage.

Login is required to use the circuit simulator.

Use Case Covered in This Article (Why Interleaved PFC Is Selected)

This article introduces an interleaved PFC as one example of a PFC circuit.
An interleaved PFC divides a boost PFC circuit into two or more phases and drives each phase with a 180° phase shift. By sharing the current between phases, device stress and heat generation are reduced.
In addition, since the inductor currents of two phases overlap, their ripple currents cancel each other out, resulting in reduced overall ripple current. Furthermore, because the effective ripple frequency increases, this approach is advantageous for input and output filter design, including ripple current and EMI.
Because the effects can be intuitively understood from the waveforms, this method is suitable for understanding and preliminary verification through waveform observation using the Online Simulator.

Login is required to use the circuit simulator.

Verification Example Using the Online Simulator (Interleaved PFC)

1. Simulation Conditions

In this simulation, the conditions shown in Figure 1 are set, and verification is carried out using TK125U60Z1, which is presented as a recommended MOSFET.

  • Input: Vin = 230V, Fin = 50Hz
  • Output: Vout = 380V, Pout = 800W
  • Switching frequency: 65kHz
  • MOSFET used: TK125U60Z1
Figure1:Interleaved PFC simulation conditions and circuit configuration

Figure1: Interleaved PFC simulation conditions and circuit configuration

2. Simulation Results

Figure 2 shows the output voltage and current, Figure 3 shows the input voltage and current, and Figure 4 shows the inductor current waveforms.
First, the output voltage waveform in Figure 2 shows that the output voltage is controlled near the target value of 380V and remains stable.

Figure2:Output voltage and output current waveforms of the Interleaved PFC

Figure2: Output voltage and output current waveforms of the Interleaved PFC

Next, the input current waveform in Figure 3 shows that the current follows the input voltage and exhibits a sinusoidal waveform. This indicates that the current waveform is corrected by the PFC circuit, and power factor correction is achieved.

Figure3:Input voltage and input current waveforms of the Interleaved PFC

Figure3: Input voltage and input current waveforms of the Interleaved PFC

Furthermore, the inductor current waveform in Figure 4 shows that the currents of inductors L1 and L2 operate with a phase shift relative to each other, confirming interleaved operation with a 180° phase difference. This indicates that the current is shared in the two-phase configuration.

Figure4:Inductor current waveforms of the Interleaved PFC showing interleaved operation with a 180-degree phase difference

Figure4: Inductor current waveforms of the Interleaved PFC showing interleaved operation with a 180-degree phase difference

3. Efficiency and Loss Evaluation in Accurate Mode

By using the Accurate mode of the Online Simulator, not only waveforms but also efficiency and device losses can be verified.
In this simulation, the following results are obtained as shown in Figure 5.

  • Efficiency: 92.2%
  • Losses
    o Q1: 1.29W
    o Q2: 1.29W

These results indicate that:

  • the two-phase configuration distributes the losses across each MOSFET;
  • the losses of Q1 and Q2 are identical, indicating that each phase shares the current evenly; and
  • the converter operates with an efficiency of approximately 92%, which is a reasonable result under the set conditions.
Figure5:Efficiency and loss evaluation results in Accurate mode

Figure5: Efficiency and loss evaluation results in Accurate mode

Specifications and Key Points of the MOSFET Used (TK125U60Z1)

The main specifications of TK125U60Z1 used in this verification are as follows.

  • N-channel power MOSFET (DTMOSVI generation), package: TOLL
  • Drain-source voltage VDSS = 600V
  • Drain current (DC) ID = 20A
  • Drain-source on-resistance RDS(ON) = 125mΩ (Max.)
  • Total gate charge Qg = 28nC (Typ.)
  • Input capacitance Ciss = 1620pF (Typ.)
  • Body diode characteristics (reference): Reverse recovery time trr = 285ns (Typ.), Reverse recovery charge Qrr = 3100nC (Typ.)

Product information (reference): TK125U60Z1

Summary

A PFC circuit reduces harmonic current by bringing the input current closer to a sinusoidal waveform and improves the power factor. The characteristics, such as current waveform, ripple, device stress, loss and efficiency, and design difficulty, vary depending on the selected topology (Single/Interleaved/Totem-Pole/Semi-Bridgeless) and current conduction mode (CCM/CRM/DCM).
By using the Online Simulator, waveforms can be compared while switching topologies, MOSFETs, and circuit parameters without environment setup or device model preparation. In addition, by using the Accurate mode, efficiency and device losses (e.g., Q1/Q2) can be evaluated, enabling quick initial design exploration.
In the interleaved PFC example presented in this article, the following can be verified in a continuous flow:
(1) current sharing with a 180° phase shift,
(2) ripple reduction,
(3) input current shaping and output voltage control, and
(4) evaluation of efficiency and losses.

Trying out an Interleaved PFC

Login is required to use the circuit simulator.

Related content

Contacts

Technical inquiry

Contact us

Contact us

Frequently Asked Questions

FAQs
A new window will open