This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Zener diodes are mainly used in constant voltage circuits and clipping circuits. Recently, it is used for protection circuits against electrostatic discharge (ESD) that apply clipping circuits.
A Zener diode is a type of pn junction diode. As the reverse bias voltage across the pn junction increases, a Zener diode enters either Zener or avalanche breakdown. This breakdown voltage increases a sharp rise as shown in Fig. 1. Reverse voltage remains nearly constant even when the reverse current changes. Because of this characteristic, Zener diodes are also called voltage regulator diodes and constant-voltage diodes.
For products, please refer to the following links.