This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Yes, it is possible to connect multiple Zener diodes in series in order to obtain a desired Zener voltage, but in this case, care should be exercised as to Zener current, Iz. For series-connected Zener diodes, the maximum allowable Zener current becomes equal to the lowest one among their specifications. Ensure that this value is not exceeded.
Furthermore, if two Zener diodes with different Zener current specifications are connected in series, one of them will not exhibit the specified Zener current and thus the specified Zener voltage.