Members Only

온라인 시뮬레이터

Update Information

Sep.2026

A new thermal simulation feature for individual MOSFETs has been added.

Sep.2026

A 3‑Phase Inverter (IPMSM) for brushless motors has been added as a new motor drive circuit simulation topology.

Aug.2026

Half-Bridge_Bridge-Rectification has been added to both the AC-DC and DC-DC converter sections.

Jul.2026

A MOSFET Gate Drive Voltage adjustment function has been added.
A PCB Illustration Window has been added to the Totem-Pole_PFC and the Semi-Bridgeless_PFC topologies of the AC‑DC Converter.

Apr.2026

A PCB Illustration Window has been added to the Single_PFC and the Interleaved_PFC sections of the AC DC converter.

Mar.2026

An H‑Bridge for Brushed DC Motors and a 3‑Phase Inverter (SPMSM) for Brushless Motors have been added in New Motor Drive Circuit Simulation target topologies.
A Semi‑Bridgeless_PFC has also been added to the AC‑DC converter in the Power Supply Circuit Simulation target topologies.

Feb.2026

A PCB Illustration Window has been added to the AC-DC and DC-DC Full-Bridge sections.

Jan.2026

A Totem-Pole_PFC topology has been added to the AC-DC converter.

Dec.2025

A PCB Illustration Window has been added to the AC-DC and DC-DC Half-Bridge sections.

Nov.2025

A Interleaved_PFC topology has been added to the AC-DC converter.

Oct.2025

A PCB Illustration Window has been added to the AC-DC and DC-DC Flyback, and the DC-DC Non-Isolated_Buck_Converter sections.

Aug.2025

A Single_PFC topology has been added to the AC-DC converter.
The feature enabling arbitrary setting of transformer parameters has been added to the Full-Bridge circuit of the AC-DC/DC-DC converter.

Jul.2025

A feature has been added to the AC-DC/DC-DC converter's half-bridge circuit, allowing the transformer parameters to be set arbitrarily.

Jun.2025

A feature has been added to the AC-DC converter’s flyback circuit, allowing the transformer parameters to be set arbitrarily.

Apr.2025

A feature has been added to the DC-DC converter's flyback circuit, allowing the transformer parameters to be set arbitrarily.

Dec.2024

Three topologies (Flyback, Half-Bridge, Full-Bridge) have been added to the DC-DC converter for the second stage of AC-DC converter.

회로 시뮬레이션

회로 시뮬레이션

Circuit Simulation is a web-based service that enables simulation of power supply and motor drive circuits directly within a web browser.
Users can evaluate waveforms, power losses, and power conversion efficiency under various conditions by changing MOSFETs and circuit parameters. This allows engineers to validate device selection and circuit designs at an early stage of development.
Because no dedicated simulation environment or device models are required, evaluation can be started quickly and easily from the initial design phase.
 

Login is required to use the circuit simulator. 

열 시뮬레이션

Thermal Simulation

Thermal Simulation is a web-based service that allows users to evaluate MOSFET thermal characteristics and heat distribution directly within a web browser.
By modifying parameters such as PCB size, MOSFET placement, heatsink configuration, and ambient temperature, users can analyze temperature distribution and junction temperature (Tj). This helps optimize thermal design and verify MOSFET selection before hardware implementation.
Since no dedicated simulation environment or thermal model preparation is required, engineers can begin thermal evaluation quickly from the early stages of product development.

Login is required to use the Thermal simulator.

Power Supply Circuit Simulation Topology List

* Simulation is recommended for use on a PC. System maintenance will take place every Tuesday from 8:00 AM to 10:00 AM (JST). During this period, the system may not operate normally.

Power Supply Type Topology Input Voltage Range (V) Output Power Range (W)

AC-DC

PFC (First Stage of AC-DC) Single_PFC 100 or 230 400 to 1600
Interleaved_PFC 100 or 230 400 to 1600
Totem-Pole_PFC 100 or 230 400 to 1600
Semi-Bridgeless_PFC 100 or 230 400 to 1600
DC-DC (Second Stage of AC-DC) Flyback 300 to 420 5 to 120
Half-Bridge 300 to 420 100 to 1600
Half-Bridge_Bridge-RectificationNEW 300 to 420 100 to 1600
Full-Bridge 300 to 420 300 to 2000

DC-DC

  Flyback 12 to 100 1 to 120
Non-Isolated_Buck_Converter 10 to 60 1 to 100
Half-Bridge 12 to 180 100 to 300
Half-Bridge_Bridge-RectificationNEW 12 to 180 100 to 300
Full-Bridge 12 to 180 200 to 500

Motor Drive Circuit Simulation Topology List

* Simulation is recommended for use on a PC. System maintenance will take place every Tuesday from 8:00 AM to 10:00 AM (JST). During this period, the system may not operate normally.

Motor Type Topology Input Voltage Range(V) Output Torque (mN*m)
Motor Drive Brushed_DC_Motor H-Bridge 9 to 48 10 to 500
Brushless_Motor 3-Phase_Inverter_SPMSM 9 to 100 10 to 2000
3-Phase_Inverter_IPMSMNEW 24 to 400 500 to 20000

Note : SPMSM (Surface Permanent Magnet Synchronous Motor)

Features

Function Introduction/Operation Procedure

문의

기술 문의

A new window will open