This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Load switch ICs are mainly used to reduce the power consumption of the system and to set the power supply sequence. In contrast, eFuse IC is used to protect the subsequent ICs and circuits from overcurrents and overvoltages when the system fails or when hot-swapping or other hot-line insertion is performed. The major differences in eFuse IC over load switch ICs are:
[Differences in eFuse IC with respect to load switch ICs]