This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
As the figure below shows, when the MOSFET is ON, current mainly flows through the coil and the MOSFET. Energy is accumulated in the coil during this time. The coil emits accumulated energy and suppresses changes of current. Current does not flow at the moment when the MOSFET turns OFF, but owing to the characteristic of this coil, current flows through a diode, and the capacitor is charged. Because of this phenomenon, output voltage exceeds input voltage.