This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
If you need to apply the input voltage after the application of an “on” signal to the CONTROL terminal, use a load switch IC with an input-tolerant function. The input-tolerant function blocks the current flowing from the CONTROL terminal to the VIN terminal when the CONTROL terminal has higher voltage than the VIN terminal or when VIN = 0V. In the case of a load switch IC without an input-tolerant function, apply the CONTROL signal following the application of VIN.
Also see the following document and web page for a description of the input-tolerant function:
To perform a parametric search of load switch ICs with an input-tolerant function for the CONTROL terminal, click:
Other load switch ICs: