This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The hold time (tHD) is a delay time that is inserted until the output is enabled. This is to prevent a malfunction due to chatter caused by the application of input voltage. When a load switch IC detects a voltage higher than the UVLO threshold and lower than the OVLO threshold, the output is enabled after the predefined delay. This function makes it possible to set the output rise time independent of the input voltage.
Also see the following document and web page for a description of hold time:
To perform a parametric search of load switch ICs with a startup hold function, click:
Other load switch ICs: