This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The true reverse-current blocking function blocks the current flowing in the reverse direction from the output terminal (VOUT) to the input terminal (VIN) when output voltage (VOUT) > input voltage (VIN), regardless of whether a load switch IC is enabled or disabled. In contrast, the reverse-current blocking function blocks this current only when a load switch IC is disabled.
Also see the following document and web page for a description of the reverse-current blocking function:
To perform a parametric search of load switch ICs with a true reverse-current blocking function, click:
To perform a parametric search of load switch ICs with a reverse-current blocking function, click:
Other load switch ICs: