This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
MOSFET on-resistances generally have thermal dependencies. Its temperature coefficient is positive. In other words, the resistance value increases at high temperatures and decreases at low temperatures.
Generally, the temperature coefficient of the resistance value of a metal conductor is positive, and the temperature coefficient of the resistance value of a semiconductor is negative. However, the temperature-coefficient of the on-resistance of MOSFET is positive. The value of the coefficient varies depending on the breakdown voltage and manufacturing process of the device, so it is necessary to check it by seeing a data sheet, etc. When designing, take this temperature fluctuation into consideration, and carry out thermal design and circuit design.
Please also refer to FAQ below for the variation of resistors.