This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The absolute maximum rated voltage is a voltage that must not be exceeded even instantaneously.
However, today's applications generate brief spikes exceeding the absolute maximum rated voltage at power-up. For these applications, the avalanche resistance may be used as a limiting parameter instead of the absolute maximum rated voltage.
The avalanche capability can only be applied when 1) the absolute maximum rated voltage is exceeded only at power-up (and is never exceeded during steady-state operation), and 2) the avalanche current is lower than the absolute maximum rated current. The avalanche capability is derated for channel temperature.
The scope of use of the avalanche capability varies from device to device. For details, contact your local Toshiba sales representative.