This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The calculation of power consumption includes, in general, power consumption due to IC bias current and power consumption due to current flowing in the output section, which are affected by the drive voltage and drive duty cycle.
〈Example calculation for a brushed motor TB67H450AFTG (from the application note)〉
The power consumed by the IC can be roughly divided into two parts: the power consumed by the transistors in the output block and the power consumed by the logic block. (Calculated with 100% drive duty below.)
P(total)=P(out)+P(bias)
Power of the output block (P(out)) is consumed by the high-side and low-side MOSFETs of the H-Bridge.
P(out)=Iout(A)×VDS(V)=Iout(A)×Iout(A)×Ron(Ω) ……………………… (1)
When the current waveform of the motor output corresponds to the ideal waveform, the average power of the output block can be provided as follows.
Assuming Ron=0.60 Ω, Iout(peak:max)=1.5 A, VM=24 V, it can be calculated as follows
P(out) =1.5(A)×1.5(A)×0.60(Ω) …………………………………………………(2)
=1.35(W)
The power consumption of the logic and IM system is calculated separately by the state of operating and stopping.
I(IM3) = 3.5 mA(typical): during operation (fPWM=30kHz)
I(IM2) = 3.0 mA(typical): when stopped (brake mode)
The output system is connected to VM (24V).
(Output system: Sum of the current consumed by the circuit connected to VM and the current consumed by the output stage switching)
Power consumption during operation can be calculated as follows.
P(bias)=24(V)×0.0035(A) ………………………………………………………(3)
=0.084(W)
From the values of formulas (2) and (3), the total power consumption P(total) during operation can be calculated as follows.
P(total)=P(out)+P(bias)=1.35+0.084=1.434(W)
The power consumption n in non-operation mode (stopping) can be calculated as follows.
P=24(V)×0.003(A)=0.072(W)
Additionally, th power consumption can also be reduced by stopping operation with standby mode (IM1=1 μA(max))
In actual motor operation, the average current will be lower than the calculated value due to the transition time of current steps and ripple caused by constant current PWM. Please refer to the above calculated values and set them with a margin after sufficient evaluation of the thermal design of the board and other components.
For individual power consumption calculations, please refer to the individual specifications or contact.
The following documents also contain related information.