This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
A leakage current flowing between the collector and emitter of the transistor at the output side of a transistor coupler is defined as Dark Current ICEO(IDARK). In this case, a current is not passed to the LED at the input side.
On the other hand, a leakage current flowing between the collector and emitter of the transistor at the output side when a low voltage (In Toshiba's case, VF=0.7V) is applied to the LED at the input side, though it is the OFF area, is defined as OFF-state Collector Current IC (off). This means that the OFF-state voltage at the input side is at a level below 0.7V.