This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
UVLO stands for Under Voltage Lock Out and refers to the undervoltage lockout function. During operation, if the power supply voltage drops and becomes lower than the UVLO detection voltage, UVLO brings the internal circuit into a semi-standby state to prevent malfunction. When the power supply voltage rises and becomes higher than the UVLO release voltage, UVLO is released and the operation restarts.
When operating a power device such as IGBT, if the gate voltage of the controlled power device drops, conduction loss increases, causing a loss increase and device destruction. A gate driver IC coupler for pre-driving such a power device may incorporate the UVLO function to control the above phenomenon.