This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Compared with a copper electric wire, optical fiber allows longer-distance transmission. Optical transmission using a single-mode quartz optical fiber supports a transmission distance of up to several tens of kilometers without a relay.
Secondly, optical transmission is less sensitive to noise. Unwanted signals other than those you want to send are generally called "noise." When you send a signal through a general electric wire, many electric devices interfere with it, causing "noise." A optical signal, however, is free from mutual interference because of its completely different nature.