This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Recently, the interface method between the main processor such as baseband and application processor and the peripheral equipment such as camera and LCD display is different, and an interface bridge that converts and connects different interfaces is required.
We provide peripheral devices such as MPD (Mobile Peripheral Devices) and IO expanders to expand the functions of the main processor as an interface bridge that supports video data transmission methods such as MIPI🄬, LVDS, DisplayPort™, HDMI🄬.
MIPI® DSI, DPI, DBI-2 LVDS, DisplayPort™, RGB
MIPI® CSI-2
HDMI®, MIPI® DSI, CSI-2
GPIO, PWM, I2C
* MIPI® is registered service marks of MIPI Alliance, Inc.
* The terms HDMI, and HDMI High-Definition Multimedia Interface, and the HDMI Logo are trademarks or registered trademarks of HDMI Licensing Administrator, Inc. in the United States and other countries.
* VESA®, DisplayPort™ and eDP™ are trademarks, service marks, registered trademarks, and/or registered service marks owned by VESA.
* DisplayPort™ and the DisplayPort™ logo are trademarks owned by the Video Electronics Standards Association (VESA®) in the United States and other countries.
* Other company names, product names, and service names may be trademarks of their respective companies.