What is the level-shift driver in high-voltage IPDs?

High-voltage IPDs receive control signals at up to 5 V from Hall-effect devices, Hall-effect sensors, and a control IC. The gate driver for the high-side device requires very high voltage equal to the sum of the high-voltage power supply (VBB) and the gate-source voltage. Because the low-voltage control signals cannot directly drive the high-side gate driver, high-voltage IPDs incorporate a level-shift driver to transfer the control signals from a low-voltage circuit to a high-voltage circuit.

Fig. 1 Example of a level-shift driver
Fig. 1 Example of a level-shift driver

The circuit, operation, and usage of high-voltage IPDs are also explained in the "Intelligent Power Device Application Note (SSOP30)". Please also refer to this document.

Related Links

The following documents also contain related information.

FAQs

Application Notes

A new window will open