This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
High-voltage IPDs receive control signals at up to 5 V from Hall-effect devices, Hall-effect sensors, and a control IC. The gate driver for the high-side device requires very high voltage equal to the sum of the high-voltage power supply (VBB) and the gate-source voltage. Because the low-voltage control signals cannot directly drive the high-side gate driver, high-voltage IPDs incorporate a level-shift driver to transfer the control signals from a low-voltage circuit to a high-voltage circuit.
The circuit, operation, and usage of high-voltage IPDs are also explained in the "Intelligent Power Device Application Note (SSOP30)". Please also refer to this document.
The following documents also contain related information.