Metals are exposed on the sides of the SSOP30 package of high-voltage IPDs. What voltage potential do they have?

The metals exposed on the sides of the SSOP30 package have the voltage potential shown below.

Fig. 1 Package Image
Fig. 1 Package Image

Related Links

The following documents also contain related information.

FAQs

Application Notes

A new window will open