At the Toshiba Innovation Centre we constantly strive to inspire you with our technologies and solutions. Discover how to place us at the heart of your innovations.
Knowledge
Highlighted Topics
Further Materials
Other
This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
CMOS logic ICs have an inverter as a standard function, and there are "04" and "U04". "04" is used for general logic processing (digital signal processing), and "U04" is mainly used for oscillators such as crystal oscillation circuits and RC oscillation circuits.
“04” and “U04” are configured as shown in Fig. 1. "04" has optimized MOS size for the required performance of input block and output. As a result, in the same group (family), the input capacitance of "04" is smaller than that of “U04”. "04" has a high gain due to its 3-stage configuration. In addition, the High-level / Low-level input voltage range (VIL, VIH) for judging "H" and "L" is wider than that of "U04" (Table 1), and the noise margin is high. However, the propagation delay time will be slightly longer.
Fig. 2 shows a conceptual diagram of an oscillator circuit that uses an inverter.
Disturbances such as noise at power-on become the seeds of oscillation and enter the input Vin. These seeds are so small that it is amplified in the linear region of the inverter, filtered in the feedback circuit and summed to the input. The conditions for oscillation are that the phase of the feedback signal is in phase with the input signal, and that the gain of the inverter is large (the magnitude of the "input" + "feedback signal" is greater than the original input signal).
“04” has a small input capacitance, so it has a wide band and high gain. It can oscillate up to a higher frequency than “U04”. Considering only this point, it seems that "04" is more suitable for oscillation than "U04". However, the linear region used for oscillation is outside the region shown in Table 1 (for example, at 4.5 V, "04" is 1.35 V to 3.15 V and "U04" is 0.90 V to 3.6 V), so "U04" is wider. The oscillation signal must circulate within this range for stable oscillation. Considering more stable oscillation at the desired frequency, it is recommended to use "U04" in the oscillation circuit.
The following documents also contain related information.
Please refer to the following e-Learning for inverter circuits and oscillation.
e-Learning:
Please refer to the following document for the basics of logic in general.
Application Notes:
Please refer to our recommended products.