This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The forward voltage, VF, of a switching diode lowers as temperature rises. The reverse leakage current, IR, increases as temperature rises.
The electrical characteristics of semiconductor devices are generally sensitive to ambient and operating junction temperatures. The characteristics of Si diodes generally change as follows in the operating range.
This is true of diodes mainly for the following reasons:
Because of a strong bond, silicon carbide (SiC), a wide-bandgap semiconductor, is affected more greatly by lattice vibration than silicon. And donor electrons are less likely to be excited in SiC than in silicon owing to a wide bandgap. Therefore, silicon and SiC diodes have different temperature characteristics in the current range in which they are normally used.
The following shows the IF–VF curves of silicon and SiC Schottky barrier diodes (SiC SBDs).
In the case of silicon SBDs, forward voltage (VF) decreases as temperature increases. Conversely, in the case of SiC SBDs, VF increases as temperature increases. At higher IF, the forward voltage (VF) of both silicon and SiC SBDs increases as temperature increases.
I explained the Schottky barrier diode as an example, but as shown in Fig. 1, pn junction diodes show the same tendency. Because of the temperature characteristics described above, silicon diodes are more susceptible to thermal runaway than SiC diodes.
In circuit design, it is necessary to take temperature dependence of electrical characteristics into consideration.
For products, please refer to the following links.