This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Diodes have two terminals, anode and cathode. Whether current flows or not depends on the direction of voltage applied to these terminals. This operation is called rectification and is the basic operation of diodes.
A diode has two terminals: an anode (positive side) and a cathode (negative side).
The diode conducts current when the voltage at the anode is higher than the voltage at the cathode by more than a value specified in a datasheet (roughly 0.7 V in the case of silicon pn junction diodes). It does not conduct current when the difference between the anode and cathode potentials is less than this value. Such action is called rectification. This diode characteristic can be used for rectifier circuits that convert direct current to alternating current (AC-DC conversion), reverse battery protection (reverse current protection), and radio wave detection.
The bias state in which the anode terminal is higher than the cathode terminal is called forward bias, and the state in which it is lower is called reverse bias.
When a reverse bias is applied to the diode and this voltage is increased, current suddenly flows at a voltage called breakdown voltage. Breakdown voltage is almost constant irrespective of current. Utilizing this characteristic, diodes are also used in constant-voltage circuits and nowadays for ESD and surge protection. However, typical diodes are subject to degradation and permanent damage when they are operated in the breakdown region. It is therefore necessary to use dedicated diodes such as Zener diodes or ESD protection diodes for these applications.
For products, please refer to the following links.