This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Zener diode is a kind of pn junction diode. When a reverse bias is applied to a pn junction diode and this reverse voltage is increased, the current increases sharply at a certain voltage (Zener voltage/breakdown voltage). A Zener diode is a diode that generates a constant voltage using this characteristic.
In general, pn junction diodes, this breakdown voltage is several tens of volts or more, but Zener diodes are products with a zener voltage of several volts to several tens of volts due to optimization of the impurity concentration of the pn junction.
In the Zener diode's breakdown region, the current increases due to two types of breakdown phenomena:
Zener diodes are used in the breakdown region above the Zener voltage. Zener diodes are used in constant voltage applications by operating in this region.
Recently, this property has been used for ESD (electrostatic discharge) protection.
Be careful not to exceed the absolute maximum ratings such as allowable dissipation values described in technical data.
Zener breakdown and avalanche breakdown are also explained in the following FAQ.
For products, please refer to the following links.