This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Absolute maximum ratings and operating condition specifications have different meanings.
Absolute maximum ratings:
This is the rated value that must not be exceeded even for a moment in order to maintain life and reliability.
Operating condition:
This is a regulation to guarantee normal operation, and it is necessary to strictly observe this condition during use.
If even one of the operating conditions is exceeded, the operation of the IC cannot be guaranteed. Either take measures to keep the rating within the range, or select another IC again.
The following documents also contain related information.