This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Power up VIN and VCT in the following sequence. Power down VIN and VCT in the order opposite to the power-up sequence.
Single-power-supply LDOs
In the case of single-power-supply LDOs, the internal control circuitry is supplied from VIN. For an LDO to work properly, VIN must be fully powered up to a nominal voltage level prior to the application of VCT.
Dual-power-supply LDOs
In the case of dual-power-supply LDOs, the internal control circuitry is supplied from the bias voltage terminal (either VBIAS or VBAT). Therefore, VBIAS or VBAT must be fully powered up to a nominal voltage level, followed by VIN and then VCT.
To perform a parametric search of single-power-supply LDOs, click:
To perform a parametric search of dual-power-supply LDOs, click: