This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Low-voltage IPDs incorporate an overcurrent protection circuit, which uses one of the three methods described below. Some IPDs achieve overcurrent protection by combining multiple methods.
See technical datasheets for information about the overcurrent protection circuit used in each IPD.
Overcurrent protection is designed for temporary protection of the IPD. Be sure to shut down a system in the event of the overcurrent protection circuit being enabled.
In the event of overcurrent detection, an internal timer starts to control the output intermittently for current limiting.
The output turns back on automatically when the overcurrent condition disappears.
In the event of overcurrent detection, the output current is limited to the programmed value.
The output turns back on automatically when the overcurrent condition disappears.
In the event of overcurrent detection, the output is turned off, and output off-state is latched.
To release the latch, apply a "L" level signal to the input terminal.