This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
In the case of the ideal op-amp, the DC voltage of the VIN(+) and VIN(-) terminals match exactly when the input voltage (Vi) is 0 V. In reality, however, there are differences in input impedance and input bias current between the VIN(+) and VIN(-) terminals, causing a slight difference in their voltages. This difference called input offset voltage is multiplied by a gain, appearing as an output voltage deviation from the ideal value.
When used in amplifiers of sensors, etc., the input offset voltage of an op-amp results in an error of sensor detection sensitivity. To keep sensing errors below a specified tolerance level, it is necessary to select an op-amp with low input offset voltage.
The following documents also contain related information: