This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Generally, load switch ICs incorporate a pull-down resistor between the CONTROL and GND terminals so that their internal circuitry remains stable in the event of the CONTROL terminal being open-circuited. Toshiba’s load switch ICs contain a MOSFET instead of a resistor as shown in Figure 1 in order to reduce control pull-down current (ICT). This MOSFET pulls down the CONTROL signal to GND with an almost constant current sink as shown in Figure 2.
Also see the following document and web page for a description of the CONTROL terminal:
Other load switch ICs: