This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Power-on MOSFET generally do not require large drive-current. However, pay attention to the current drive capability,in the case of high-speed switching.
Bipolar transistors require a large base current to maintain a low on-state voltage. However, MOSFET is a voltage-controlled device, so it can be driven with only small amount of power to charge the gate. However, since the input capacitance Ciss of the powered MOSFET is somewhat large, the input capacitance must be charged quickly with a low-impedance drive circuitry, particularly for high-speed switching.
As a guide to the gate-current required for recharging, the drive-current can be calculated simply from Qg properties specified on the datasheet. If the required switching-time is t (desired), for example ton or toff, then:
Ig=Qg/t(desired)
The application note "Electrical characteristics: Power MOSFET application note" has charge-capacitance characteristics. Please also refer to this.