This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Increasing the gate-resistor Rgate connected to the outside of MOSFET slows the switching-up and suppresses inrush current.
Generally, large capacitor Co for voltage stabilization is connected to the output side of the MOSFET.
When the MOSFET turns on, inrush current IRUSH flows to charge this capacitor.
This inrush current is reduced by increasing the series gate resistor Rgate.
When the gate resistance increases, the rising output current becomes less pronounced.
However, if increasing gate resistance affects the switching speed and loss, it is necessary to select the suitable gate resistance on your using condition. Refer to the following application notes for details on how to determine the gate resistance.
Document: MOSFET Gate Drive Circuit Application Note (PDF:1.56MB)