This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Figure 1 shows a simple BRT circuit. RO is a pull-up resistor for the BRT, and ZL is the load impedance. For the sake of simplicity, ZL is considered an impedance (resistance) expressed as a real number.
In this case, while Q is on, the collector-emitter voltage must satisfy the low-level voltage requirement for the following circuit.
First, let’s consider a circuit without ZL.
Without ZL, the collector-emitter saturation voltage (VCE(sat)) of the internal transistor (Q) is expressed as a function of the collector current (IC):
VCE(sat) ≈ RO * IC
When ZL is connected to the BRT, the combined impedance seen from the collector of the BRT is:
Z = RO // ZL = RO * ZL / ( RO + ZL )
The collector-emitter voltage (VCE) due to this combined impedance is expressed as follows:
VCE = Z * IC
VCE must satisfy the low-level voltage requirement of the following circuit. Otherwise, it is necessary to increase the collector current by increasing the base current (Ib) of the internal transistor.
Ib can be increased in the following ways:
1. Increase the input voltage (VI).
2. Replace the BRT with the one having a smaller R1 value.
3. Replace the BRT with the one having a larger R2 value.