This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
A bias resistor built-in transistor (BRT) is a bipolar transistor with a bias network consisting of a series base resistor and a base-emitter resistor. With bias resistors built into the transistor, BRTs help reduce the number of external components required, simplifying a discrete circuit configuration. BRTs are commonly used for switching applications.
Recently, there is a tendency to use MOSFETs instead of transistors with built-in resistors owing to their high-speed switching, low current consumption, on-voltage, low drive voltage, etc.