This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
While IGBTs and other bipolar devices(*1) are on, carrier injection into the high-resistance drift region causes its resistivity to decrease. This is called conductivity modulation.
The N- drift region in IGBTs and other high-voltage switching devices is thick and has low dopant concentration. Therefore, the N- drift region has extremely high resistivity. The IGBT turns on when the gate-emitter and collector-emitter paths are positively biased as shown below. At this time, holes are injected into the N- region from the collector P region via the N region. Consequently, the carrier concentration in the high-resistance N- region increases, causing its resistivity to decrease. As a result, its forward voltage drop decreases, causing the IGBT to act as a switching device with low on-state voltage.
This increase in conductivity (i.e., a reduction in resistivity) during a conduction period is called conductivity modulation.
(*1) A bipolar device is a type of semiconductor device that uses both electrons and holes as charge carriers for current conduction. In contrast, unipolar devices such as MOSFETs use only one type of charge carrier.