This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
In principle, photorelays can be used by series connections and by parallel connections. However, there are important points that require attention. For series connections, voltage sharing between devices (distribution, balance) is important. Especially, within the transition time when the state shifts from OFF to ON or ON to OFF, in time differences that occur between devices connected in series, voltages must be balanced so that a voltage exceeding the value for OFF-state output terminal voltage VOFF is not applied.
For parallel connections, current sharing between devices (distribution, balance) is important. Especially in the ON state, currents must be balanced so that ON-state currents flowing between devices connected in parallel do not become unbalanced or not exceed the specified value for ON-state current ION.