This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The current with the threshold value for the photo triac to turn ON when the current passed to the LED is increased is defined as trigger LED current (IFT). It varies with the product. The maximum value for such a variation is specified with IFT(Max). However, this does not mean that in circuit designing, LED current IF must not exceed this Max value. In designing IF, , also by considering LED deterioration over time, temperature, and design margin, a value for IF larger than IFT (Max) must be set.
For details, also refer to Toshiba Application Note "Triac couplers-basic properties and application design", section 9.1 How to design the input-side LED current IF. For IF, the maximum rating including temperature derating is also specified, and whether or not such a rating is exceeded must be checked.
(https://toshiba.semicon-storage.com/ap-en/semiconductor/knowledge/application-note.html)