This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
When using a triac coupler as a trigger device for the main triac, a load current directly flows through the triac coupler until the main triac turns on. When using zero-cross triac-output photocouplers, since the voltage when they are turned ON is kept low, current limiting resistor RT does not have to be inserted. When using non-zero-cross triac-output photocouplers, a large current flows. The current limiting resistor must therefore be defined as Peak ON-State Current or ON-State Current (Pulsed) (ITP or IONP), and designed not to exceed the value specified for the maximum rating (2A as an example). In general, Toshiba recommends that the current be controlled at about half of the rated current. For 100VAC power supplies, 100Ω is recommended, and for 200VAC power supplies, 200Ω is recommended.
How to design RT also described in Toshiba Application Note "Triac couplers-basic properties and application design", section 9.5.
(https://toshiba.semicon-storage.com/ap-en/semiconductor/knowledge/application-note.html)