This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
With the advent of an advanced information society, the amount of information handled every day has dramatically increased, and the increase in power consumed by data centers and information and communications equipment has become a problem on a global scale. Therefore, the demand of high-efficiency for switched-mode power supply (SMPS) that supply power to data centers and information and communications equipment has been increasing in recent years.
The loss of MOSFET in switched-mode power supply is roughly divided into on-time loss and on-off switchover loss, the new generation DTMOSVI 650 V series aims at improvement focusing on reduction of the switchover loss. Especially aiming the loss reduction by speed up the switching from ON to OFF, the new generation reduces the values of “drain-source On-resistance x gate-drain charge” by about 40 % compared with the previous generation [Note 1]. And this reduction allows the efficiency of switching power supplies to be improved by about 0.36 %[Note 2].
TOLL is a surface-mount package that has an approximately 27 % smaller footprint than the usual D2PAK package. It is also a 4-pin type package that allows Kelvin connection of its signal source terminal for the gate drive. This can reduce the influence by the inductance of the source wire in the package to bring out the high-speed switching performance of the MOSFETs, suppressing oscillation when switching.
Toshiba will continue expanding its product lineup to meet market trends and help improve the efficiency of power supplies.
[Note 1] the new generation DTMOSVI prepares several patterns of the product of “drain-source On-resistance x gate-drain charge” from 40mΩ×27nC to 210mΩ×7.1nC. It is possible to select the appropriate parts according to the application and design concept, including package variations.
[Note 2] As of July 2021, values measured by Toshiba (When TK040N65Z in the new series is compared with TK62N60X in the conventional series by using a PFC circuit with an output power of 2500 W)
* The values mentioned in bracket under the product names are RDS(ON) Max /ID Max
Package |
Qgd typ. (nC) |
||||
|---|---|---|---|---|---|
|
|
|
|
|
|
8.0×8.0×0.85 |
10.0×15.0×4.5 |
15.94×20.95×5.02 |
15.94×20.95×5.0 |
9.9×11.68×2.3 |
|
TK210V65Z |
TK190A65Z |
TK190U65Z (0.19Ω/15A) |
7.1 |
||
TK170V65Z |
TK155A65Z |
TK155U65Z (0.155Ω/18A) |
8 |
||
TK125V65Z |
TK110A65Z |
TK110N65Z |
TK110Z65Z |
TK110U65Z (0.11Ω/24A) |
11 |
TK099V65Z |
TK090A65Z |
TK090N65Z |
TK090Z65Z |
TK090U65Z (0.09Ω/30A) |
12 |
TK065N65Z |
TK065Z65Z |
TK065U65Z (0.065Ω/38A) |
17 |
||
TK040N65Z |
TK040Z65Z |
27 |
|||