This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
PWM (Pulse Width Modulation) is used to control electric power inside the motor coil.
The output power is controlled by repeatedly turning the output ON and OFF.
Constant voltage operates the motor with the constant period of the pulses.
The resulting voltage in the motor coil depends on the width of the voltage pulses.
It utilizes the semiconductor feature that ON/OFF states have the least loss while the intermediate state has the most loss.
PWM control is widely used in inverter circuits because of its excellent controllability and high efficiency.
It is also used to control brushed DC motors.
In the inverter circuit, AC voltage of a sine-wave that is optimal for driving the motor can be created by periodically changing the ON state (duty) of PWM control.