This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The tool consisting of the hardware and the software and used for the test is called an emulator. It debugs the executable programs written by users.
By using an emulator, the software executes for each instruction, checks the operation, and reads and writes data in the memories and registers. It is possible to check the operation in various situations.
Emulators can be roughly categorized into two types: an in-circuit emulator and an on-chip debug emulator.
An on-chip debug emulator can debug in an environment that is close to the actual machine since it uses the on-chip debug function of the microcontroller incorporated on the target system.
On the other hand, the in-circuit emulator realizes high functionality by using the microcontroller for the emulator separated from the actual microcontroller.