Low Power Consumption Control Block

Low Power Consumption Control Block

TX03 series microcontrollers control the low power consumption mode by using a Clock Generator block (CG block) that controls the clock supply and the external interrupt signal.

  • In low power consumption mode control, the standby operation mode including clock supply and clock stop is controlled.
  • It converts the external interrupt signal to the high active signal and requests an interrupt.
    5 interrupt signal types (High, Low, Rising edge, Falling edge, and Both edges) can be supported.

Chapter 3 Peripheral Circuits

Low Power Consumption Technology
Low Power Consumption Mode (1)
Low Power Consumption Mode (2)
Peripheral Circuits by Group of TX3
Peripheral Circuits of the M320 Group
M320 Group Application Example
3-7. Peripheral Circuits of the M330 Group
M330 Group Application Example (1)
M330 Group Application Example (2)
Peripheral Circuits of the M340 Group
M340 Group Application Example
Peripheral Circuits of the M360 Group
M360 Group Application Example
Peripheral Circuits of the M390 Group
M390 Group Application Example
Peripheral Circuits of the M370 Group
M370 Group Application Example
Overview of Vector Engine (VE)
Peripheral Circuits of the M380 Group
M380 Group Application Example (1)
M380 Group Application Example (2)

* Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.

A new window will open