How to calculate the junction temperature of a semiconductor device whose datasheets do not include a “thermal resistance” value

At first, the value of “thermal resistance Rth(j-a)” is calculated by using the datasheet data below. The ambient temperature shall be 25 [deg.C].
Rth(j-a) = (Tj(max) – 25 [deg.C]) / PC
Tj(max): Junction temperature in Absolute Maximum Ratings
PC: Collector power dissipation in Absolute Maximum Ratings

Junction temperature is calculated by using the above thermal resistance.
ΔTj [deg.C]= Rth(j-a) [deg.C/W] × PLOSS [W]
Tj = ΔTj + Ta
ΔTj: Junction temperature rise
Rth(j-a): Thermal resistance, junction to ambient
PLOSS: Power dissipation in semiconductor device
Tj: Junction temperature
Ta: Ambient temperature

For a semiconductor device package used with a heat sink, in order to ensure more accurate calculations, thermal resistance of junction-to-case values should be used instead of thermal resistance of junction-to-ambient values.
In this example, it is calculable by the same formula as above by using PC values @ Tc = 25 [deg.C].

For the meanings of symbols, please see below.

  • Bipolar Transistor
    Junction temperature : Tj  
    Thermal resistance : Rth(j-a), Rth(j-c)  
    Collector power dissipation : PC
  • MOSFET
    Channel temperature : Tch 
    Thermal resistance : Rth(ch-a), Rth(ch-c) 
    Drain power dissipation : PD

For calculation of junction temperature, please refer to “Thermal Design and Attachment of a Thermal Fin: Power MOSFET Application Notes”

A new window will open