This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
At first, the value of “thermal resistance Rth(j-a)” is calculated by using the datasheet data below. The ambient temperature shall be 25 [deg.C].
Rth(j-a) = (Tj(max) – 25 [deg.C]) / PC
Tj(max): Junction temperature in Absolute Maximum Ratings
PC: Collector power dissipation in Absolute Maximum Ratings
Junction temperature is calculated by using the above thermal resistance.
ΔTj [deg.C]= Rth(j-a) [deg.C/W] × PLOSS [W]
Tj = ΔTj + Ta
ΔTj: Junction temperature rise
Rth(j-a): Thermal resistance, junction to ambient
PLOSS: Power dissipation in semiconductor device
Tj: Junction temperature
Ta: Ambient temperature
For a semiconductor device package used with a heat sink, in order to ensure more accurate calculations, thermal resistance of junction-to-case values should be used instead of thermal resistance of junction-to-ambient values.
In this example, it is calculable by the same formula as above by using PC values @ Tc = 25 [deg.C].
For the meanings of symbols, please see below.
For calculation of junction temperature, please refer to “Thermal Design and Attachment of a Thermal Fin: Power MOSFET Application Notes”