This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
When the electrically charged human body and an electronic device come into contact with each other, static electricity is discharged into the electronic device. The most common points of electrostatic discharge (ESD) entry include USB, HDMI®, power supply, and other connector ports. ESD also enters from an antenna with exposed metal surfaces.
TVS diodes must be connected to all the data and power lines that need to be protected from ESD. TVS diodes should be placed as close as possible to the ESD entry points.
We provide an extensive lineup of TVS diodes, including single-bit TVS diodes and multi-bit TVS diode arrays. Our product lineup also includes TVS diode arrays with a flow-through pin arrangement that are designed for much-requested USB, HDMI®, and other multi-ports to simplify board trace layout. Select TVS diodes according to the signal frequency, circuit configuration, and board layout.
* The terms HDMI, and HDMI High-Definition Multimedia Interface, and the HDMI Logo are trademarks or registered trademarks of HDMI Licensing Administrator, Inc. in the United States and other countries.
* Other company names, product names, and service names may be trademarks of their respective companies.