This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
To suppress the inrush current that occurs when the load switch IC is enabled, use a load switch IC with an inrush current limiting function, which suppresses the current flowing to the capacitor connected to the output terminal (VOUT) by slowing turning on the output-stage transistor. The inrush current limiting function is also called a soft-start, slow-start, or slew rate control function.
Please also refer to the following documents for related explanations.
Application note
FAQ
To product list of load switch ICs :
Main web page about load switch ICs
Other information