This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Discrete semiconductor devices have no concept of operating temperature. This is because, the current flowing through the element and the applied voltage differ depending on the customer's circuit and conditions, and the amount of heat generated cannot be defined by the ambient temperature and power supply voltage. For this reason, in discrete devices, instead of the operating temperature range, the absolute maximum rated channel temperature (or junction temperature) is specified for the upper limit of the device temperature, and the storage temperature is specified for the lower limit. Please use within this temperature range.
The following documents also contain related information.