This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
When static electricity is applied to the motor driver’s control pins, the input circuits may be damaged or destroyed.
Generally, the oxide film used in input pins for motor drivers is very thin (few nano meter level), therefore when a static electricity of few hundred to few thousand volts is applied, the device will be damaged or destroyed.
Our devices have integrated surge protection circuits/elements for each input pins, but it does not guarantee that the device will not be damaged under any circumstances. Please avoid static electricity to be applied to the device directly.
When handling semiconductor products, be sure that the environment is protected against static electricity. Operators should wear anti-static clothing, anti-static shoes, and a wrist strap. In addition, containers and other objects that come in direct contact with semiconductor products should be made of materials that do not produce static electricity that would cause damage.
Control anti-static equipment at all times to ensure that it works correctly. Take utmost care when handling semiconductor devices with ESD warning labels.
For general static electricity countermeasures, please refer to the page below.
The following documents also contain related information.