This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The history of motors began with the discovery of electromagnetic phenomena in the early 19th century.
So far, numerous types of motors have been developed including direct current (DC) motors, induction motors, and synchronous motors.
Brushless motors have a long history as permanent magnetic synchronic motors (PMSM), but they have not been used except for industrial applications with expensive control mechanisms due to the difficulties in starting and changing speed.
In recent years, brushless motors have been rapidly developed for a wide range of fields, due to the development of strong permanent magnets, the ease of inverter control by semiconductor elements, and the increased awareness of energy conservation.