This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The speed of a brushless motor is adjusted by changing the voltage.
The rotation speed is increased by raising the voltage and increasing the frequency of the drive command waveform.
If only the frequency of the drive command waveform is increased, the rotation of the rotor will not be able to follow and the rotor will stop.
Also, if only the voltage is increased, the rotor will rotate faster, but the frequency of the drive command waveform will be too slow to stop the rotor.
Therefore, it is necessary to adjust both the voltage and drive command waveform.
(The frequency of the drive command waveform of the brushless motor is determined by the position detection of the rotor.)